Where can I get pre and post-transfer signals on series 300 with Group G controller?
To have pre and post-transfer signals available, feature 31 needs to be enabled.
For Series 300, a set of form C contacts are provided on the group G controller as "OP1".

When the feature setting of "OP1" is set to operate the contacts as "Feature 31", the time delay settings of the pre and post-transfer signals are available.

For further information, refer to page 11 of the Group G controller user's guide. If unsure, contact Technical Support at 1-800-800-ASCO or send an email to technicalsupport@ascopower.com
For Series 300, a set of form C contacts are provided on the group G controller as "OP1".
When the feature setting of "OP1" is set to operate the contacts as "Feature 31", the time delay settings of the pre and post-transfer signals are available.
For further information, refer to page 11 of the Group G controller user's guide. If unsure, contact Technical Support at 1-800-800-ASCO or send an email to technicalsupport@ascopower.com
Released for: Schneider Electric Saudi Arabia