Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can I use voltage signal on AI3 of the ATV320?
Issue:
Customer has 40Vdc input connected on AI3 analog input of ATV320.

Product Line:
ATV320

Environment:
All model numbers, all serial numbers

Cause:
ATV320 didn't follow the voltage input signal on AI3

Resolution:
No, AI3 input of the ATV320 only accept 0-20mA or 4-20mA current signal.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre