EcoStruxure Process Expert [2020]: Error while placing an object in supervision edit mode
This can happen with the versions like HDCS2018 R2,HDCS 2019 & EPE 2020 R1.
In the above scenario, the user has to replace the Vjc.Project.Client.dll in the folder C:\Program Files\Schneider Electric\EcoStruxure\Process Expert(HDCS)\Engineering Client\ with the corrected .dll file which is provided by EPE R&D team. Later, the user must perform the page editing and save operation in full screen mode of supervision.
For the .dll file, please contact ecostruxure-hybrid-dcs.support@schneider-electric.com.
Released for: Schneider Electric Saudi Arabia