Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What can replace a 920?
If you have any of the LEGACY ASCO 920 Remote Control Switches shown on the table below.
The current replacement for this is the NEW ASCO 920 Remote Control Switch.

Please take note that the mounting measurements may not be the same.

image.png
For further information, you may click on this 920 link or contact Technical Support at 1-800-800-2726 then dial 3 or send an email to technicalsupport@ascopower.com.