Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is CF12 fault on the ATV600 and ATV900 Process drives?

Article available in these languages: Spanish

Issue:
What can cause a CF12 fault on the ATV600 and ATV900 Process drives?

Product Line:
ATV600 and ATV900

Environment:
All

Cause:
Corrupt file in HMI

Resolution:
"Conf transfer Error"
Principle:
The Configuration transfer error occurs if a configuration file could not be loaded to the device, or the config. is not compatible with the drive.
Probable cause:
• The configuration transfer to the drive was not successful or interrupted.
• The stored configuration (HMI) was loaded from an different firmware (MCP/MCE)
Remedy:
• Load a compatible configuration.
• Use SoMove to transfer configuration to an other drive.
• Perform a factory setting"