How can we help you today?

Is there a way to Freewheel Stop on Profinet with Process Drives?

Issue:
How can you do a freewheel stop on the ATV630 and ATV930 over Profinet command?

Product Line:
ATV630, ATV930 Series with Profinet option card.

Environment:
All

Cause:
Want the drive to freewheel stop when command is coming from the Profinet network.

Resolution:
CMD or command bits 0 and 1 both have set to 0 at the same time to command a freewheel stop over the Profinet network.

Schneider Electric Saudi Arabia