How can we help you today?

Can Start and Stop be performed with an Analog signal on ATV212 drive?

Issue:
Can I start and stop the ATV212 drive with a 4-20ma analog signal?

Product Line:
ATV212

Environment:
All

Cause:
No Start Stop control signal on VFD

Resolution:
No. The start and stop (forward / reverse) commands should be controlled with digital inputs (+24Vdc only).

Schneider Electric Saudi Arabia