Search FAQs
Osisense XC - Is the XCMD2116L2 limit switch available to order?
The XCMD2116L2 limit switch does not exist as a commercial reference in complete limit switch
How to get it
- by ordering the following sub-assemblies ZCMD21L2 body + ZCE01 head + ZCY16 steel roller lever, and assemble them (2-pole NC + NO Snap Action)
- by ordering XCMD2116C12 limit switch with 5-pin M12 connector (4A-60V), having 2-pole NC + NO snap action and pre-wired 5-pin M12 connector 2m cable length to order separately
Released for:Schneider Electric Saudi Arabia
Explore more
Explore more