Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the I/O be configured through the display of an PM8000 series meter?
Issue
The PM8000 has onboard I/O and/or expansion I/O that needs to be configured in order to work.

Product Line
PM8000

Environment
ION Setup

Resolution
The I/O has to be configured through ION Setup and cannot be configured through the display or webpages of the PM8000.

You can download the latest version of ION Setup here: ION setup latest revision

Please see related article: Video: How to configure the PM8000 digital inputs using ION Setup