Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can you export a project to local computer in EcoStruxure Power Build - Easy Series application
Issue: Steps to Export an EPB Easy Series project to your local system.
Product Line: EcoStruxure Power Build easy Series.
Cause: Projects can be exported to manage and update project information.
Resolution:
You can export an existing project in two different ways:
  1. Go to home page of EPB Easy Series after you create project
- you can see your project on screen, then click on three dots on right top corner of your project field.
- Then click on “Export as File” to download your project
Export screen
  1. Once the project is created you can download your project from Project information screen by clicking on download symbol next to “Project Name” which is placed on top left side of the screen.
Download project screen