Issue:
I need an IP41 Resi9 MP enclosure.
Product Line:
Resi9 MP
Resolution:
Yes, thanks to an additional kit resi9 MP can reach IP41 in both installation, flush and surface.
Notes:
The commercial reference of the IP41 additional kit is MIP99034.
Instruction Sheet BBV48376
I need an IP41 Resi9 MP enclosure.
Product Line:
Resi9 MP
Resolution:
Yes, thanks to an additional kit resi9 MP can reach IP41 in both installation, flush and surface.
Notes:
The commercial reference of the IP41 additional kit is MIP99034.
Instruction Sheet BBV48376
Released for: Schneider Electric Saudi Arabia