Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is electrical endurance ( E0-E1-E2) of the downstream Earthing Switch of DMVL-A (24KV) cubicle?
Issue:
what is the electrical endurance of the down stream earthing switch of DMVL-A cubicle at 24KV
SM6 general characteristics

Resolution:
The downstream Earthing Switch of the DMVL-A cubicle at rated voltage 24KV has electrical endurance of class E2.

More Information  about Earthing Switch electrical endurance and its classifications can be found in the below FAQ:

>> https://www.se.com/ng/en/faqs/FAQ000233932/