How can we help you today?

Is there a way to detect when the value of a variable has changed ?

Issue:
Detecting the a change in value of a variable


Product Line:
Unity Pro, EcoStruxure Control Expert


Resolution:
Yes, Attached is a DFB that allow the detection of when a variable of type INT or REAL value has changed

Schneider Electric Saudi Arabia

Attachment(s)
variable_value change detection_dfb.xdb [2.79 KB]