How can we help you today?

In Modbus RTU transmission, what communication parameters does an ASCO device supports?

Transmission Format
Although the Modbus protocol supports both ASCII and RTU modes of transmission, only the RTU mode is implemented. Within the RTU mode, the ASCO devices supports the following communication
parameters:
  • 8 data bits
  • no parity
  • 1 stop bit

Reference: Page 1 of Connectivity to the ASCO Power Manager Xp & 7000 Series Group 5 Controller via Modbus 381339-221
For further questions and document requests, you may send your inquiry to technicalsupport@ascopower.com or Contact 1.800.800.ASCO (2726).

Schneider Electric Saudi Arabia

Attachment(s)
381339-221O.pdf [358.97 KB]