How can we help you today?

How Prisma Range Switchboards are categorized in Ecostruxure power design- Ecodial?

In Ecodial, Below is the categorization of Prisma Switchboards.
The criteria to Select Prisma G Range Switchboards in Ecodial are as below. The criteria to Select Prisma P Range Switchboards in Ecodial are as below
When the requirement of the electrical switchboards areWhen the requirement of the electrical switchboards are
up to 630A,up to 4000A,
When Isc is Upto 50kA,When Isc is Upto 100kA rms/1s,
IEC61439-1&2 CompliantIEC61439-1&2 Compliant
The switchboard will continue operating as intended even in severe earthquake conditions.
The criteria to Select Prisma G Active Range Switchboards in Ecodial are as below The criteria to Select Prisma P Active Range Switchboards in Ecodial are as below
When the requirement of the electrical switchboards areWhen the requirement of the electrical switchboards are
up to 630A,up to 4000A,
When Isc is upto 50kA,When Isc is Upto 100kA rms/1s,
IEC61439-1&2 Compliant &IEC61439-1&2 Compliant &
Communicable smart panelsCommunicable smart panels
PrismaSeT Active is the newest generation of low-voltage switchboards featuring native connectivity to the cloud. This revolutionary approach lets any customer, in any commercial building, give their electrical distribution a voice. Fast commissioning makes installs more efficient, and real-time smart alarms optimize maintenance and improve uptime. The switchboard will continue operating as intended even in severe earthquake conditions.

Schneider Electric Saudi Arabia