Setting up PID auto/manual for ATV12 drive
Issue:
Setting up PID auto/manual for ATV12 drive
Product Line:
Altivar 12
Environment:
All
Cause:
N/A
Resolution:
Go under CONF, FULL, FUN, PID-, and set PAU to the digital input needed.
Next, set PIN setting to manual reference needed. Options are no, AI1, or A1U1.
Released for: Schneider Electric Saudi Arabia