Is Sepam 2000 discontinued & what is the replacements for that?
Issue:
Sepam 2000 availability.
Product Line:
Sepam 2000
Resolution:
Yes, Sepam 2000 is discontinued and spare parts are not available to order.
Replacement will be sepam 40/60/80 series or you can use Micom /P3/P5 according to application.
Details can be reachable through our SE site www.se.com.
Sepam 2000 availability.
Product Line:
Sepam 2000
Resolution:
Yes, Sepam 2000 is discontinued and spare parts are not available to order.
Replacement will be sepam 40/60/80 series or you can use Micom /P3/P5 according to application.
Details can be reachable through our SE site www.se.com.
Released for: Schneider Electric Saudi Arabia