Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Wiring & Programming Status Relays R1 & R2 on the ATV340 Drive
Issue:
How are the relays for ATV340 drive programmed?

Product Line:
Altivar 340

Cause:
Relay programming.

Resolution:
2 relays available R1 and R2.
R1 can be wired as normally-open (R1A and R1C) or normally-closed (R1B and R1C).
R2 is normally-open only.

To program relays:
[Complete settings] -> [Input/Output] -> [Relay] -> [R1 configuration] or [R2 configuration], depending on preference.

See attachment for relay programming, relay delay time, relay active at, holding time, and relay fall back assignments.

Schneider Electric Saudi Arabia

Attachment(s)
Relay Configuration ATV340.pdf [655.01 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre