How can we help you today?

What is the firmware version of the ATV630 and ATV930 Drives that offers the ethernet cybersecurity features?

Issue:

ATV630 and ATV930 Drives that offers the cybersecurity features with what firmware version?

Product Line:

ATV630 and ATV900 open and enclosed.

Environment:

All

Cause:

Cyber Security for Ethernet

Resolution:

ATV630 Firmware version v3.3IE34 and above have the Ethernet cybersecurity.

ATV930 Firmware version v3.1IE27 and above have the Ethernet cybersecurity.

Schneider Electric Saudi Arabia