Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Unable to install PLC-USB driver due to user conflict
Installing the 'SchneiderPLCUSBDriverSuite V14.15.0.0' returns the following error.:
PLCUSB Driver

Use the following steps to run the ps1 file named 'Release-PerUserDrivers.ps1' can be used to resolve the issue.

  • Browse to the location you stored the ps1-file in File Explorer and choose; File-> Open Windows PowerShell.
  • Type (part of) the name of the script.
  • Press TAB to auto complete then name. Note: Do this even when you typed the name in full. ...
  • Press ENTER to execute the script.
Note: This doesn’t uninstall the old driver versions, but it deletes any 'SchneiderPLCUSBDriverSuite' installer related
registry keys that causes Windows to detect and refuse the install/uninstall of the driver components..

Schneider Electric Saudi Arabia

Attachment(s)
Release-PerUserDrivers.ps1.txt [16.07 KB]