Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How are the units setup when reading Modbus address 3204 Motor current?

Issue:

Customer is not getting back what he expects when reading motor current 3204 over Modbus.

Product Line:

Altivar drives

Environment:

All

Cause:

Reading Modbus register 3204

Resolution:

Register 3204, Motor current, reads in tenths. Example 200 = 20.0A.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre