How can we help you today?

In VAMP 321, What is the next step to be done after physically connecting the arc sensors and the I/O units to the relay?

Issue,
Customer want to know what is the next step to be done after connecting the sensors to the I/O unit

Resolution:
VAMP 321

Environment:
After physically connecting the sensors and the I/O units to VAMP 321 relay, the following steps must be done. These steps are to be done at the beginning of the project installation and repeated after adding or removing any sensor or I/O unit at any time.

1- Make sure you are connected to the relay
2- In VAMPset, Go to Arc protection menu
image 1

3- Go to "Install arc sensors & I/O units " menu and select install.
image 2

4- "Installation state' is then changed from ready to installing
image 3

5- when installation is finished, the installation state will go back to ready.

Schneider Electric Saudi Arabia
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
Need help?

Need help?

Product Selector

Product Selector

Quickly and easily find the right products and accessories for your applications.

Get a Quote

Get a Quote

Start your sales enquiry online and an expert will connect with you.

Where to buy?

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

Help Centre

Help Centre

Find support resources for all your needs, in one place.