Which kind of ethernet cable shall I used for cabling a remote I/O ethernet architecture on M580 configuration .
Schneider-Electric recommends the use of SFTP (Shielded and Foil Twisted Pair) Cat5e or Cat6 (10/100 Mbps) cables, especially the cables listed below :
- TCSECN3M3M••••: Cat 5E Ethernet straight-through shielded cable, rated for industrial use,,CE- or UL-compliant
- TCSECE3M3M••••: Cat 5E Ethernet straight-through shielded cable, rated for industrial use, CE-compliant
- TCSECU3M3M••••: Cat 5E Ethernet straight-through shielded cable, rated for industrial use, UL-compliant
Released for: Schneider Electric Saudi Arabia