- Both TRANSFER SWITCH position lights are flashing (this indicates an error condition).
- Count the number of times the Automatic Generator Exerciser light flashes (repeats after a pause). This number is the error code.
- Error codes:
3 light flashes - Generator failed after starting. See generator manual.
4 light flashes- Generator over frequency. See generator manual.
5 light flashes - Transfer Switch did not transfer the load to the generator. (Service required)
6 light flashes - Transfer Switch did not transfer the load to the utility. (Service required)
7 light flashes - Controller error (Service required)
- To clear the error code, press and release the Push to Test button.
For further information, please refer to page 8 of operator's manual 381333-163 or contact 1-800-800-2726 then dial 3 for Technical Support.
Released for: Schneider Electric Saudi Arabia