How can we help you today?

What are files with the extension .HMIX?

Issue
Where do files with the file extension .HMIX come from?

Product Line
Vijeo Designer
Intelligent Data Services

Environment
HMI Configuration Software

Resolution
.HMIX extension files are exported from Vijeo Designer HMI applications that are used to create solutions for an add-on called Intelligent Data Services (IDS). IDS is a tool that runs on a Windows Server that is used to comply with FDA Electronic Records and Electronic Signatures standard "CFR 21 Part 11". for the Food and Pharmaceuticals industry.

To perform this export:
1) Right-click on the name of the HMI ("Target1" is the default name)
2) Choose "Export..." from the context menu
Vijeo Designer Target Export
A Validation of the project will occur.

3) Save the file:
Save As screen

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Saudi Arabia