How can we help you today?

How to conduct a generator test without load transfer for a 165 Series ATS?

During the test, the generator cranks and starts, and the GENERATOR light comes on (if it is acceptable). After running for 20minutes it stops. Throughout the test, the load remains connected to the utility (the automatic transfer switch does not transfer the load to the generator).

165 Control Panel Test Button.jpg

1. Press and release (do not hold) the Push to Test button. The generator cranks and starts and the GENERATOR acceptable light comes on and stays on.

2. The generator runs for 20 minutes. The automatic transfer switch does not transfer the load to the generator. The TRANSFER SWITCH on the utility (preferred source) light stays on.

3. To bypass the time delay or cancel the test, press and release the Push to Test button again.

4. The generator stops and the GENERATOR acceptable light goes off.

For further information, you may contact Technical Support at 1-800-800-2726 then dial 3 or send an email to technicalsupport@ascopower.com.

Schneider Electric Saudi Arabia