Issue:
What is an INFL error on the ATV340 drive?
Product Line:
Altivar 340
Environment:
All
Cause:
Internal time clock error. Communication error between keypad and drive or a clock oscillator start failure.
Resolution:
Reinitialize the communication by following steps.
- Power off the drive and wait until display is blank and repower on to confirm issue.
- Disconnect keypad from the drive and remove batter if applicable.
- If problem persists, try a different keypad if possible.
Released for: Schneider Electric Saudi Arabia