How can we help you today?

Can the ATV212 be used at high elevation?

Issue:

Customer wants to use the ATV212 at elevation over the maximum elevation listed in the Manual (1000 meters).

Product Line:

Altivar 212

Environment:

Altitude over 1000 meters

Cause:

High elevation jobsite

Resolution:

The ATV212 products is limited at 1000m without derating.

You can reach 3000m with current derating 1 % per 100m.

The limit is 2000m for Corner grounded system.

We can not be higher because the rated insulation of the product is designed for altitude up to 3000m.

Schneider Electric Saudi Arabia