What is the priority of use between sockets TE and T2S on EVlink Pro AC ?
If the connectors on the T2 and TE sockets are connected at the same time, the T2 socket has priority over the domestic socket.
If the authentication mode is free charging without lock or charging without badge with cable lock and you disconnect one connector, the second connector will automatically be powered.
For other modes you have to relaunch the charging session.
If the authentication mode is free charging without lock or charging without badge with cable lock and you disconnect one connector, the second connector will automatically be powered.
For other modes you have to relaunch the charging session.
Released for: Schneider Electric Saudi Arabia