How can I make a Modbus register Read Only in a .CSV symbol table file for OFS server?
Issue:
Making a Modbus register Read Only in a .CSV symbol table file for OFS server
Product Line:
OFS Server
Resolution:
In the CSV file you would add a postfix ;R for Read Only in the same cell at the Modbus register, example : 400008;R
see image below

As you can see, the registers with the postfix ;R is read only

The variables are "read only" only in the OFS Server.
Making a Modbus register Read Only in a .CSV symbol table file for OFS server
Product Line:
OFS Server
Resolution:
In the CSV file you would add a postfix ;R for Read Only in the same cell at the Modbus register, example : 400008;R
see image below
As you can see, the registers with the postfix ;R is read only
The variables are "read only" only in the OFS Server.
Released for: Schneider Electric Saudi Arabia