How can we help you today?

Minimum length of the ethernet copper cable for the HSBY port on the M580

Issue
What is the minimum length of the ethernet copper cable for the HSBY port on the M580?

Product Line
M580 processors

Resolution
If you are using a 100Base-T or below connection the recommended minimum length is 1 meter (3.28 ft), if you are using a 1000Base-T connection then there is no specified minimum length.

Schneider Electric Saudi Arabia