How can we help you today?

How to online M340 via BMXNOM0200 through ModbusTCP gateway in Control Expert ?

Issue:

How to online M340 via BMXNOM0200 through ModbusTCP gateway in Control Expert ?

Product Line:

M340

Environment:

EcoStruxure Control Expert

Resolution:
The address syntax could be expressed as ModbusTCP_Gateway_IP;BMXNOM0200_slave_number

In this sample, the 192.168.10.20 is the IP address of ModbusTCP_Gateway, which could be accessed by the PC where the control expert is installed. One channel of BMXNOM0200 should be configured as a Modbus slave with address 1 and it should be wired to the Modbus link of the ModbusTCP gateway.

SNAP1.JPG

Schneider Electric Saudi Arabia