How can we help you today?

What is the insulation resistance and dielectric strength test for BMXFCA300?

Issue
What is the insulation resistance and dielectric strength test for BMXFCA300?

Product line
X80 I/O Modules SUB-D Connector

Environment
BMXFCA300

Resolution
The insulation resistance test is 20 ohms per kilometer and the dielectric strength is 1000VDC.

Schneider Electric Saudi Arabia