Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the insulation resistance and dielectric strength test for BMXFCC303?
Issue
What is the insulation resistance and dielectric strength test for BMXFCC303?

Product line
X80 I/O Modules SUB-D Connector

Environment
BMXFCC303

Resolution
The insulation resistance test is 20 ohms per kilometer and the dielectric strength is 1000VDC.