How can I prevent / inhibit the Series 7000 Bypass Transfer Switch from switching over to Emergency power?
There are several ways to go about this.


- Turn the Emergency power source off (If this cannot be done, please see #2 or #3).
- Turn the BYPASS handle to connect the bypass switch to the NORMAL source.
- If the Automatic Transfer Switch with Bypass and Isolation switch came with either one of these optional accessories, 30** or 34B, either one can be used to prevent the switch from connecting to the Emergency source.
Released for: Schneider Electric Saudi Arabia