What replaces the LC breaker in an I-line interior?
Issue:
Needs to replace a LC breaker in an I-line interior
Product Line:
I-line circuit breaker
Environment:
Legacy LC frame
Cause:
LC Obsolete
Resolution:
The MJA breaker replaces the LC, however the MJA requires 9" of space where the LC only used 7.5", so they would need an additional 1-1/2" of mounting space in the I-line section per breaker.
Released for: Schneider Electric Saudi Arabia