Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does Vijeo Designer support Harmony P6?
Harmony P6 is a new iPC range and it is supported by Vijeo Designer as a Harmony iPC from the version VJD 6.2 SP12.
The goal of this article is to inform about registration policy and the target model.

This article is applicable to the following products:
Harmony P6

This topic is related to Vijeo Designer and Vijeo Designer Runtime for Windows

The Harmony P6 has been tested and validated with Vijeo Designer as a Harmony iPC from the version VJD 6.2 SP12.
Below, please find the License type and the Target Model for the Harmony P6 from VJD 6.2 SP12.

The License type and the Target Model for the Harmony P6 from VJD 6.2 SP12

Schneider Electric Saudi Arabia

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: