How can we help you today?

Is it possible to simulate IO Scanner Objects, such as the TM3BCEIP, in EcoStruxure Machine Expert - Basic simulator?

Issue:
Is it possible to simulate IO Scanner Objects, such as the TM3BCEIP, in EcoStruxure Machine Expert - Basic simulator?


Product Line:

EcoStruxure Machine Expert - Basic (V1.0, V1.1, V1.2)


Resolution:

No. IO Scanner objects, such as the TM3BCEIP, are not simulated while running the simulator of Machine Expert - Basic.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Saudi Arabia