Does the EcoStruxure OPC UA server Expert allow dynamic IP address of the computer without a repair setup for the certificate update?
Issue:
Dynamic IP address for OPC UA Server Expert
Product Line:
EcoStruxure OPC UA Server Expert
Resolution:
Yes, The OPC UA server will support the use of dynamic IP address by way of the /dynamicip command line parameter.. This allows the server to ignore IP address machine modification that would require a setup repair for certificate update. This will help to manage certificates with dynamic IP. To allow dynamic IP, run the command OPCUAServerExpert.exe /dynamicip.
Released for: Schneider Electric Saudi Arabia