Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the fire classification of EVlink Pro AC ?
Concerning fire classification the IEC 61851-1 call the IEC 61439-7 that call the IEC 61439-1.
EVlink Pro AC respect the §10.2.3.2 of this last standard.

Standard extract