Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is accessory 31BG?
Accessory 31BG is a Status Relay Bundle that provides a relay (3 total) for each of the following statuses:
  • Normal Source Acceptability
  • Emergency Source Acceptability
  • Pre & Post Transfer Signal
Each relay has 2 NO/NC (Form C) sets of contacts rated for 6A at 120Vac, 250Vac Max.

Please see below for a more detailed accessory description and screen short from a sample wiring diagram.
31BG accessory description

31BG wiring diagram
Please click here for the Group 5 Control Panel User's Guide

For further information you contact Technical Support at 1-800-800-2726 then dial 3 or send an email to technicalsupport@ascopower.com.