How can we help you today?

Browser compatibility with SAGE

Issue

Sage RTU with old firmware is not compatible with newer browsers.

Product Line

Sage 2300, Sage 2400, Sage 3000 Sage 3030.

Environment

Power Metering device, front display.

Resolution

Open Microsoft Edge and enter the IP address for the RTU unit. Then press the Icon for compatibility mode. This is a workaround but it may not work with your current browser version.

Internet Explorer compatibility mode

A more permanent solution is the Offline Editor or the CPU upgrade. Contact technical support or your sales rep for more information.

Phone: 888-797-6468 (888-PWR-MGMT) Option 7, or

E-mail: sagertu_support@schneider-electric.com

Schneider Electric Saudi Arabia