Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the programming cable for the XBTN200 Magelis HMI?
Issue:
Programming cable for XBTN200 Magelis HMI


Product Line:
XBTL1000, XBTN200


Resolution:
The programming cable for the XBTN200 is the  TSXCUSB485 + XBTZ925

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: