Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to fix the issue of not being able to install EcoStruxure Automation Device Maintenance version 3.1.129?

Issue

When installing EcoStruxure Automation Device Maintenance version V3.1.129 to replace the previous version already installed, the installation wizard displays the progress of the installation and at the end there is this message error below.

Also, the Windows Installer log file created during installation mentions a few errors at the end of the process.

Installation Wizard of EcoStruxure Automation Device Maintenance V3.1.129

Windows Installer log file

Product Line

Modicon M340, Modicon M580, Modicon Momentum, Module d’E/S Modicon X80.

Environment

Windows 10 Pro, Schneider Electric Software Update V.2.6.3.

Resolution

This issue is fixed with latest EADM 3.1.130. Please download it via SESU.