How can we help you today?

Can DC and AC X80 CPS modules be installed in a power supply redundancy rack ?

Issue:

Can DC and AC X80 CPS modules be installed in a power supply redundancy rack ?

Product Line:

X80

Environment:

X80

Resolution:

This is possible to mix DC and AC CPS modules in the BMEXBP0602 and BMEXBP1002   rack.

Each redundant CPS is able to deliver 3.3Vdc and 24Vdc to the whole drop.

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: