How can we help you today?

Can BMXART0814 support non-isolated TC ?

Issue:

Can BMXART0814 support non-isolated TC  ?

Product Line:

X80

Environment:

EcoStruxure Control Expert

Resolution:

BMXART0814 could support non-isolated TC ,however "broken wire test " option of the non-isolated TC should be disabled.

demo

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: