How can we help you today?

Can the "change password" option be disabled from the default login screen in EOTE?

Issue
Don't want users changing the password during runtime.

Product Line
Operator Terminal Expert 3.3 SP1 and older

Cause
The default login screen allows any user to change passwords during runtime, which might not be desirable.

Resolution
The default login screen in EOTE can not be modified, but it is possible to create a custom login screen.

To create a custom login screen you will need the following tool chest parts:

  • 3 Text box
  • 2 String Display
  • 2 Switch

Example

TextBox1: "User:"
TextBox2: "Password:"
TextBox3: "Invalid username or password" Note: This is optional

StringDisplay1, current value: Target01.SecuritySettings.UserNameEnter RedBox
StringDisplay2, current value: Target01.SecuritySettings.PasswordEnter RedBox

Scripts
Options for Login Script
Option 1: Just for Login.

Login1 Script

Option 2: Login + Invaid Username or password message.
Target Variable: Target01.SecuritySettings.CurrentSecurityLevel.

Login2 Script

Logout script

Logout Script

Optional Script
It automatically changes the screen to a different one after a successful login.
The Target variable used on both instances of the script is: Target01.SecuritySettings.CurrentSecurityLevel.
On the Change Screen, choose the Screen ID of your preference

Change Screen Script

Schneider Electric Saudi Arabia