Issue
Seeing this error when installing.
Resolution
- Shorten the PC name to less than 15 characters
- Restart the PC
- Re-install EcoStruxure Control Expert v15.3
- Insure you can launch EcoStruxure Control Expert v15.3 Classic or Topology Manager
- Change the PC name back to its original length
- Restart the PC
- Insure you can launch EcoStruxure Control Expert v15.3 Classic or Topology Manager
If you continue to have issues installing EcoStruxure Control Expert v15.3, please contact support either VIA chat from www.se.com, email customer.services@se.com or call 888-266-8705.
Released for:Schneider Electric Saudi Arabia