Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can IO Scanner be modified in an M580 Hot Standby system without interruption?

Issue

Looking to add, remove or modify devices from the NOC or CPU DTM. Can this be done without process interruption?

Resolution

Yes, this can be done. As of Unity V12, all Control Expert and v2.8 of M580, the ability to apply an offline application modification and return to a Standby state was introduced.  This is accomplished using the HSBY_BUILD_OFFLINE block. It supports modifications that require an offline BUILD CHANGE. It will not support ReBuild All modifications, only Build Change.

Attached is a document which outlines this feature.

Schneider Electric Saudi Arabia

Attachment(s)
M580 HSBY Adding a Device while Process Running v2.0.pptx.zip [997.18 KB]