Where can I find the ATS01 Type 1 and Type 2 coordination table?
Please note that Type 2 coordination is not available for the ATS01. However, the Type 1 coordination table is provided below and outlines the corresponding part numbers for all components required to achieve Type 1 coordination.
Reference: The Type 1 coordination table can be found in the attached ATS01 catalog (refer to page 9).
Released for: Schneider Electric Saudi Arabia